Hi,
I have a system consisting of one ZC, one ZR and one ZED. My problem is that if the system is up and running, then the ZC is turned off and later turned on, then the ZC doesn't (re)join the network. When the ZC starts, it broadcasts a "Beacon Request" and the ZR replies with a Beacon response. Apparently that makes the ZC think that there already exists a network with that PAN ID (I use fixed PAN ID), and the ZC reports a "Network Startup Failure" to the application and stops. The Beacon response from the ZR does (correctly) indicate that the ZR isn't a PAN coordinator itself. Does anybody know what the correct scenario would be? I mean, is it the ZC or ZR that does something wrong in this situation since it doesn't "simply work"?