This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

serial port interface commands - Not getting response

Hi - I have compiled SampleApp - EndDeviceDB with the following compiler options:

CC2430DB
REFLECTOR
HAL_UART
INT_HEAP_LEN=4096
ZAPP_P1
ZTOOL_P1
MT_TASK
SERIAL_RX_INT
SERIAL_TX_INT
MT_USER_TEST_FUNC
MT_NWK_PING
MT_NWK_FUNC
MT_ZDO_MGMT
MT_ZDO_FUNC
xMT_AF_FUNC
MT_ZDO_FUNC
MT_ZDO_MGMT

On Z-Tool,  I want to run  ZDO_NWKADDR_REQUEST   to get the 16 bit network address of the device.  While running this command on Z-tool, I select the following message parameters: 

IEEE address :  9943967850384659991  ( this is decimal equivalent of the device address  0x8A00121314151617. z-tool doesn't accept hex number)

reqType  SINGLE_DEVICE_RESPONSE

security Enable  NOT_ENABLED

start index 0

But ,  when  I run the command ( send message) ZDO_NWKADDR_REQUEST ,   I get following resopnse which does not contail the 16 bit address

 

<TX>7:18:11.672 COM1 ZDO_NETWORKADDRESS_REQUEST (0x0A02)
IEEEAddress: 0x8A00121314151617
ReqType: SINGLE_DEVICE_RESPONSE (0x0)
StartIndex: 0x00
SecurityEnable: NOT_ENABLED (0x0)

<RX>7:18:11.687 COM1 ZDO_NETWORKADDRESS_RESPONSE (0x1A02)
Status: SUCCESS (0x0)
 

Please tell me if somethin is missing..   I need to find the 16 bit address as it is reqired for most of other serial commands : (  

I know it has somethin to do with the following statement :

"You must subscribe to 'ZDO IEEE Address Response'  to receive the data response to this message"

please clarify what does this stmt mean ?

-Mahan