Hi..
I'm working with cc2430db.I want it to interface with the serial port of the PC where the zigbee packets are written to the serial port and read from the PC.
1) I went through the Serialapp application provided,tried building it using IAR but I got the following errors:Fatal Error[e163]: The command line symbol "_EXTENDED_STACK_END" in C:\Texas Instruments\ZStack-1.4.3-1.2.1\Projects\zstack\Utilities\SerialApp\CC2430DB\..\..\..\Tools\CC2430DB\f8w2430.xcl 197
-Z(XDATA)EXT_STACK+_EXTENDED_STACK_SIZE=_EXTENDED_STACK_START-_EXTENDED_STACK_END is
not defined.
Error while running Linker.
How to Proceed?
2) How to begin to build applications using Z-Stack from the scratch?I went through many application examples but many functions are utilized from many files...Is there any resource as to how to build these applications from the scratch?
Kindly help me as to how to proceed.
Looking forward for the suggestions,
With regards,
Swaroopa.