Other Parts Discussed in Thread: CC2431, CC2430
Hi,
I have some problems,
1. How to read RSSI in CC2431?
2. How to transmit RSSI to my PC and save it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Andy Lo said:1. How to read RSSI in CC2431?
You can use the CC2430 datasheet to get information regarding the RSSI status register to read for a local RSSI value. This is found on the CC2430 Product Folder.
Andy Lo said:
2. How to transmit RSSI to my PC and save it?
What protocol stack are you using?
If the ZStack, there is an example application called SimpleApp which could be modified to transmit the RSSI value over the Zigbee network from a remote device and have the Collector send this data over a UART interface to the PC.
If you are using a SimplicTI stack, you can also use one of the example applications provided with the SimplicTI stack download.