This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The maximum data transferred, and how to do this

Hi All,

I have read that the maximum bytes transfered is 102 Bytes without any securities and coding. If I, however, try to send approx. 90 Bytes with the help of the command AF_DataRequest, the data is not transfered. Is it possible to use this method for this data transfer? I did not find any constraint of AF_DataRequest in the manual.. If this method is not correct, can you write me right method..

Thank you for your help..