This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ZB_BIND_CONFIRM - unknown status value

Hi everybody,

I'm a bit confused about a status value, which I get from ZB_BIND_CONFIRM. It is 0x21 and I can't find it in the CC2480 Specs. Any ideas on that?

Thanks in avance!

Best regards,

Jan

  • Hi Jan Gampe,

    Do u still have that problem???

    It might give wrong status values, bcoz may be ur zstack not started, means u have to get start confirm call back with the status value zero. Make sure of SapiAppRegister command and StartRequest Command, the Rx start Confirm Callback and see the status value. If it's zsuccess u'll get ZB_BIND_CONFIRM correctly.

    Also, suppose if u want a router to bind with a co-ordinator  u need to keep a co-ordinator in ALLOW_BIND mode by filling timeout byte as oxFF. If there is any device in the n/w in allowBinding mode then router or end device will bind to it, then it'll give BIND_CONFIRM with correct status value.

    Make sure of SapiAppRegister,  StartRequest  and  start_confirm u'll get bind_confirm.

    Hope it helps.........