This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Zigbee and MSP430F149

Other Parts Discussed in Thread: MSP430F149, Z-STACK

Greetings ,

 I don't have a lot of experience on networking, communication, or hardware. I'm currently working on a class project that  sends information from the computer using Windows into a micro controller connected to an LCD that will show that information. I plan to make that communication from PC to micro controller wireless. I've been doing some research about diferent wireless technology I could do this. I'm very interested in using Zigbee to develop this project. I will be using an IT micro controller msp430f149 and the LCD will be Hyundai # HG25504. I was wondering if I could get information about how the information will be transfered from the computer to the micro controller using Zigbee. Do you know any reference I could use or someone I could contact that could help me with this?

Your help will be greatly appreciated,

Josue

  • My recommendation would be to purchase the CC2520DK, which comes with two nodes, and you can start experimenting with the Z-Stack 2.1.0 software which you can
    download from free. You will need to purchase an IAR license though.

    If you must, there is also the 99 bucks CC2480 kit...