For the reference design of the folded dipole given in Application note AN040, what is the pcb thickness to be used for fr4 substrate?
Can we use solder mask dielectric above the pcb antena?
if we use it , Will it reduce the range?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For the reference design of the folded dipole given in Application note AN040, what is the pcb thickness to be used for fr4 substrate?
Can we use solder mask dielectric above the pcb antena?
if we use it , Will it reduce the range?
Hello Saumya,
If you download the reference design from the website, you will find a readme file included with the PCB layer description. Regarding the dielectric .. have a look at our designs/EM ... you should notice that there is indeed dielectric over the antenna trace.
http://focus.ti.com/docs/toolsw/folders/print/cc2430em_refdes.html
FILE: CC2400EM_FD_REFERENCE_DESIGN_1_31.ZIP PACKED WITH WinZIP PACKED WITH WinZIP
PCB DESCRIPTION:4 LAYER PCB 1.0 MM NOMINAL THICKNESS WITH 0.35um Cu PER LAYER
DIELECTRIC FR4
Dielectric constant for FR4 is 4.5
Dimensions in manufacturing files are in mils (0.001 inch)
DOUBLE SIDE SOLDER MASK,
DOUBLE SIDE SILKSCREEN,
5 MIL MIN TRACE WIDTH AND 8 MIL MIN ISOLATION.
Hope this helps!
Cheers,
Yoda