This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reducing the rejoin time for end devices

This is an optimization of a problem I have posted here (http://community.ti.com/forums/p/2949/11417.aspx)

Right now I am able to toggle when the end deivce will rejoin or not. However we obsever that even if I put the duration of the rejoin to 500ms we are still seeing that one rejoin cycle is longer than that duration.

I did some investigation and determined that in ZDO_StartDevice it uses a global, zgDefaultStartingScanDuration, to set the scan duration of each rejoin.

Can you then tell me what is the valid boundary of this variable? At default it is set to STARTING_SCAN_DURATION (5).

I am doing some experimenation now to determine if reducing it to 1 or 0 will minimize the rejoin duration.

But any feedback will be greatly appreciated.