This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Z-Stack fragmentation

Other Parts Discussed in Thread: CC2430, Z-STACK

Hi there, we are currently working with the Z-Stack 1.4.2 for CC2430 platform and we are wondering if the segmentation is implemented in that version of the stack. We did try the Transmit application you provide among the utilities but the application seems to work only with max data length 102 and we did not succeed in using the fragmentation feature that seems to be supported.  Does anybody know if that functionality is supported and, if yes, how we should set the application up to have it working?THANKS!