This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eZ430-RF2480 UART parameters

What UART parameters should one use to connect to the USB UART emulator that is shipped with the eZ430-2480 demo kit?  According to the posts that I've read, the baud rate is 19200.  How about the parity, stop bits, flow control, etc?

Also, should I expect the data to be in plaintext (ASCII)?  I've read several accounts of people using it with hyperterminal, and using the command set outlined in the CC2480 documentation.

Thanks in advance.