Sorry for my bad english first!
I'm using z-stack 1.4.3 with CC2430.
Now I setup a network,which has 2 router and 2 end device:
2 router:their short Address are 0x0001 AND 0x007A
0x0001 has two children :0x006B AND 0x006C
0x007A has no child
On the end device ,I use NLME_GetCoordShortAddr() to get the parent address,and it works,reports the right short address 0x0001
After the following operations,I get the problem
I turn off the power of 0x0001,After a while ,that 2 end device re-connect to router 0x007A,and get the new address 0x004E AND 0x004F
But,NLME_GetCoordShortAddr() still report that both the 2 End device's parent address is 0x0001(I'm sure I have updated the parent address,Every time before the End device sends out the message,it uses the API NLME_GetCoordShortAddr() for once)
Can someone help me with this problem? thanks!!!