Hi everybody!
I'm facing a weird problem with smartrf04eb + SoC Debug Plugin. First of all I have read the same kind of thread about "no em detected" but this is little bit different. I have few prototypes which are, of course, identical. Everyone of them has has been working ok, since things started to go wrong. "no em detected" occurs with every other board except one. I read, once again, CC2430 data sheet very carefully and I know that two rising edges forces the debug mode while RESET_N is kept low. But what happens before that. What is the method that smartrf04eb concludes that there is no em connected to it? LED2, LED3, LED4 just goes on and this familiar text appears on the lcd screen. IAR workbench doesn't have an affect on this. My project configuration is ok, also been working fine before this so there is no lock options enabled.
If I can't use flash programmer or IAR workbench with my CC2430, is there any way to force cc2430 to clear everything. I was thinking that there might be "some bit crosswise".
I have connected vcc from smartrf04eb I/0 port 0 (3.3V) to my prototype + plug in module(debug interface pin2). Things have been working with this kind of connection fine before this day. I suppose debug pin2 is used to inform smartrf04eb to set right voltage level.
CC2430 is working fine because when I connect a battery to my prototype it starts to do its things.
I hope this is enough for you to see what my problem is. If someone knows what I should do please tell me, I would appreciate it.
-Antero