This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

POLL RATE and Low Power of CC2430

Other Parts Discussed in Thread: Z-STACK, CC2430

Hej!

I am going on with low power on CC2430. I followed Application Note AN053 "Measuing power consumption with CC2430& Z-Stack" to learn low power application. It worked well when I set everything exactly the same as this document says. One exception is that I use the Zstack 1.4.3-1.2.1 while the Zstack 1.4.1 by measurement in Application Note.

The problem is that: low power is arrived(the same result as shown in the document),  only when the POLL RATE is set to 500(same as specified in this note). When I set it to 1000 or other value, a constant current value is gained as result.

This comes the same when I try my own project. POLL RATE 500 is the only setting to get low power!

What is the probelm to me? Please, please give me some advice I am nearly crazy!