This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Node Power Descriptor

I would like to make some changes on the default Node Power Descriptor and I'm not sure about the following definitions:

For what is the definition of the power level? TX-power influence?:

// Power Level
#define NODEPOWER_LEVEL_CRITICAL    0x00  // Critical
#define NODEPOWER_LEVEL_33              0x04  // 33%
#define NODEPOWER_LEVEL_66              0x08  // 66%
#define NODEPOWER_LEVEL_100            0x0C  // 100%

Why is there a difference between rechargable and disposable batteries?:

// Node Available Power Sources (AVAILPWR) - bit map
//   Can be used for AvailablePowerSources or CurrentPowerSource
#define NODEAVAILPWR_MAINS            0x01  // Constant (Mains) power
#define NODEAVAILPWR_RECHARGE      0x02  // Rechargeable Battery
#define NODEAVAILPWR_DISPOSE        0x04  // Disposable Battery