This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Setting Device Capacity in Beacon Payload in TI ZStack?



Hi,

               We are using TI's C2431DK board and ZStack-1.4.3-1.2.1 ZigBee Stack.

We have some queries regarding the software modules, the queries are as follows :

         1. Which API to use to modify the DeviceCapacity and RouterCapacity in beacon payload?

         2. Which API to use to modify the transmit power?

         3. To run the sample switch-lamp application on the battery boards i.e. using the push-button switch and LED available on the battery boards, what modifications are to be made?

         4. By default, whether TI stack supports ZigBee 2006 or ZigBee PRO. How to change the same in the code?

Thanks,

Saravanan.N