This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can Zigbee stack on CC2480 be upgraded



Presently the CC2480 ships with the Zigbee 2006. The Zigbee 2007 stack is already released so question is can I as an end user upgrade the version of the stack.

From what I can figure out, the CC2480 is based on the CC2430F128, and therefore my guess is possible that it should be possible to reflash the part with different versions of the Zigbee stack. If one cannot update the firmware, how will TI add additional features as the Zigbee stack evolves.

Then another question. Do TI have any plans to release an AT Command mode for the CC2480; then it could be used as a wireless modem. I know some other vendors, eg Maxstream offer such a mode. Very handy I must say.