Other Parts Discussed in Thread: Z-STACK, CC2430
Hi All,
I would like to use the Z-tool interface on the cc2430 (using z-stack), and I have three questions:
1. Is it possible to use the CTS / RTS signals while using the z-tool. What and where should I change the code?
2. How do I change the UART speed of the MCU to 115200 bps?
3. Can I set the UART speed to more than 115200 bps?
thanks,
Nir