Other Parts Discussed in Thread: Z-STACK
Hi
I found the discussion on Keil versus IAR very interesting. I am using CC2480 for my project. I am familiar with AVR and CodeVision compiler. I am using CCS for DSP. I need advise/feedback on the flexibility and cost benefits of using any particular compiler/MCU combination for my project. If I decide to use MSP430 then is it better to go for IAR or CCE. With AVR I would prefer to use CodeVision.
Also can the CC2480 operate as a standalone device. It has GPIO/ADC and if I want to use these featurers why do I have to use another MCU. It would be better if I just send the command (ON/OFF) to CC2480 over the air and it should toggle the respective IO. There will be cost benefit [cost of MCU removed] if its just operating as an end device.
Regards
Vdevan