Other Parts Discussed in Thread: Z-STACK
Hi, I found a mistake in the CC2480 Interface Specification. The mistake in page 49 in section 6.5.28.2 The description to the function and to the fields in the frame are wrong. I send an email to the support and I report the mistake. But they don't tell me the right descriptions. I think the function is to send a command to a node that it has to leave the network. But I can't find a list of options, which I should put into the last filed in the frame. Maybe anyone can help me.