Other Parts Discussed in Thread: Z-STACK, SIMPLICITI, TIMAC
Hi, I am currently trying to use beacons in Z-Stack 1.4.3 on a SmartRF04EB with a CC2431EM installed and several CC2431EM+battery boards. However when I set the stack to use beacons the Coordinator (the SmartRF board) hangs where it displays the IEEE address on the LCD and doesn't get any further. If I use ZTool I can see that Devicestate is DEV_COORD_STARTING. I think that I have set the stack up correctly, I am using the NETWORK_SPECIFIC stack profile ID and set NWK_MODE to NWK_MODE_STAR in nwk_globals.h and have set DEFAULT_BEACON_ORDER and DEFAULT_SUPERFRAME_ORDER in ZDapp.c to 6 and 2 respectively. From what I have picked up from the documentation this is all I should need to set to get beacons working however I can't seem to get them working.
Any help on the matter would be much appreciated.
Regards Arrian.