This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SAPI ZB_SEND_DATA_REQUEST question

Hi, i need more information about the CommandID and the Handle. What kind of values should i write in? I read the interface Specification (SWRA175A), but i can't find information about it. The lenh field is the length in byte of the data, which i want to transfer, right? Before i'am able to transfer data a simple descriptor must be created, i think. Is this the responding function to create a simple descriptor? =>ZB_APP_REGISTER_REQUEST Is someone here who is able to give me an example? Thanks.