Other Parts Discussed in Thread: CC2430, Z-STACK, CC2530
Our company has bought the CC2430 Development Kit (Rev 1.4) and we are using the
TI-Zigbee-Zstack-1.4.2-1.1.0 for our development.We are also interested
on the Over Air Download (OAD).With the help of the Support- Document of
Zstack and the help-document of ZOAD, I have added the ZportApp
application to my own project,compiled the new project successfully, maked
to binary file and download onto the board. When I connected the board and
the host PC with a serial line and run the ZOAD, it always poped a message
window showing "no host device avaliable ".How can I deal with it? Is the
"Over the Air Download Evaluation Module Kit " necessary for the OAD ?
By the way ,in some document I saw some information on ZNetwor which can show
the topology of the Zigbee network, how can I get it?