Other Parts Discussed in Thread: CC2530, CC2590
I cannot get PAEN and EN signals out of the 2530 to properly handle the 2590, they are both high all the time. I can run xmit receive tests via RF studio successfully and all looks good, low error rates and good transmissions ranges. I am using P1_5 as the connection to EN on the 2590 and P1_2 as the connection to PAEN. The following setting are used within are code and these values are also used within RF Studio: RFC_OBS_CTRL0 = 0x068; OBSSEL2 = 0xFB; RFC_OBS_CTRL1 = 0x6A; OBSSEL5 = 0xFC; I am also using the HAL_PA_LNA_2590 compiler option. I can connect two devices but the power is very power and the connection range is not even 10 feet. I verified that the PAEN and EN signals are both high(the not allowed section of the truth table for these signals). I searched other postings on this topic and found about 1/2 a dozen but not a one that had any resolution, and so I type here. I'd appreciate any comments any readers may have, Thanks.