Other Parts Discussed in Thread: CC2591, CC2530, CC2590
Hi all,
I am trying to make CC2530 work with CC2591,but no success.Please can someone help me look into the problem and tell me what wrong I am doing.My work details are1> I am using Zsatck 2.5.0.2> Software changes done are :Enabled HAL_PA_LNA switch,also changed my PAEN(OBSSEL2) & EN(OBSSEL3) according to hardware(P1_2 & P1_3),and using 0_7 as HGM & LGM.The RFC_OBS_CTRLx register are default with the values given in the stack.When I build and run the project,I get the device type as cordinator but dont see any beacon request packets(on packet sniffer running on separate module) sent by cordinator.Please note that the same project runs well when without CC2591 support and reverting back the above mentioned software changes.My hardware design team has not design the hardware according to the TI reference design,its a two layer board with some components missing.When asked about their design they said that they took help from a vendor company of TI.I have attached the sch here and please let me know the complicationsthat I might face with the hardware design.Thanks for reading my mail.