This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Coordinator channel scan selection in Z stack 2.5.0(multiple configuration)?

I found the problem will be multiple definitions of scan channel list:

 

In nwk_global.h:

 

Channel mask

#define MAX_CHANNELS_868MHZ     0x00000001

#define MAX_CHANNELS_915MHZ     0x000007FE

 

#if !defined ( MAX_CHANNELS_24GHZ )

  #define MAX_CHANNELS_24GHZ    0x07FFF800

#endif

 

In nwk.h

#define DEF_CHANNEL_SCAN_BITMAP  MAX_CHANNELS_24GHZ

 

In f8wConfig.cfg

/* Default channel is Channel 11 - 0x0B */

// Channels are defined in the following:

//         0      : 868 MHz     0x00000001

//         1 - 10 : 915 MHz     0x000007FE

//        11 - 26 : 2.4 GHz     0x07FFF800

//

//-DMAX_CHANNELS_868MHZ     0x00000001

//-DMAX_CHANNELS_915MHZ     0x000007FE

//-DMAX_CHANNELS_24GHZ      0x07FFF800

//-DDEFAULT_CHANLIST=0x04000000  // 26 - 0x1A

//-DDEFAULT_CHANLIST=0x02000000  // 25 - 0x19

//-DDEFAULT_CHANLIST=0x01000000  // 24 - 0x18

//-DDEFAULT_CHANLIST=0x00800000  // 23 - 0x17

//-DDEFAULT_CHANLIST=0x00400000  // 22 - 0x16

//-DDEFAULT_CHANLIST=0x00200000  // 21 - 0x15

//-DDEFAULT_CHANLIST=0x00100000  // 20 - 0x14

//-DDEFAULT_CHANLIST=0x00080000  // 19 - 0x13

//-DDEFAULT_CHANLIST=0x00040000  // 18 - 0x12

//-DDEFAULT_CHANLIST=0x00020000  // 17 - 0x11

//-DDEFAULT_CHANLIST=0x00010000  // 16 - 0x10

//-DDEFAULT_CHANLIST=0x00008000  // 15 - 0x0F

//-DDEFAULT_CHANLIST=0x00004000  // 14 - 0x0E

//-DDEFAULT_CHANLIST=0x00002000  // 13 - 0x0D

//-DDEFAULT_CHANLIST=0x00001000  // 12 - 0x0C

//-DDEFAULT_CHANLIST=0x00000800  // 11 - 0x0B

-DDEFAULT_CHANLIST=MAX_CHANNELS_24GHZ

 

It seems I can only enable MAX_CHANNELS_24GHZ in nwk_global.h, otherwise it will have error(like I define it in f8wConfig), also if I don't want energy scan and want stick to one channel, I need to change both DEFAULT_CHANLIST in f8wConfig and DEF_CHANNEL_SCAN_BITMAP in nwk.h?

thanks

Rui