This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error using RS232 interface of cc2530 DK

Other Parts Discussed in Thread: Z-STACK, CC2530, CC-DEBUGGER

hi

i was using serial port of cc2530dk Eb....while running z-stack sample application " Serial App"......upon debugging I receoved error

Fri May 18 03:37:47 2012: Warning: No target selected, session aborted.
Fri May 18 03:37:49 2012: Fatal error: Unknown exception in driver (#E1)   Session aborted!
Fri May 18 03:37:49 2012: Failed to load debugee: C:\Texas Instruments\ZStack-CC2530-2.4.0-1.4.0\Projects\zstack\Utilities\SerialApp\CC2530DB\EndDeviceEB\
Exe\SerialApp.d51

kindly reply how to solve????reply fast plz

  • Wow - it looks like you guys are pulling an all-nighter based on the timestamp of the IAR diagnostic message ... is this project due today?

    Anyway, I have seen this when the target board gets disconnected from the PC or the USB otherwise loses sync - sometimes a usb hub port expander bogs down and you have to unplug and replug into the PC the usb hub, sometimes just cycle power and reconnect the target board, sometimes re-boot the PC.

  • yup u took it right project is due on 26th and our whole work is left with zigbeeeeee :( and no help

    sorry thats nt the case ,actuallyy when we connect the hardware of cc2530 with usb cable it works   ,but when we connect the device using serial port of evalution board it display the message "no TARGET selected" and device have no acess to the PC even in the device manger... so plx guide us what the problem is? and how to solve

    thanx for replying

    regards..

     

  • The IAR debugger only connects via USB cable to SmartRF05EB or the CC-Debugger - IAR debugger can never use a serial port connection.