This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430EXP5438A + CC2530 running Z-Stack sample applications

Other Parts Discussed in Thread: CC2530, Z-STACK

Dear all, 

I am trying to execute the sample application in Z-Stack for EXP5438A board. I have two EXP5438A boards each connected with one CC2530.

When I execute the sample application, I see that both red and yellow LEDS blink continuously. When I press SW1 as mentioned, both stop blinking. When I press them again, they switch on and after a second they turn off. When I press Sw1 again, red LED turns on and after time of one second it turns off. The same thing also happens with Coordinator. I dont know why yellow LED doesnt blink at all (which means I dont receive any data). I have made sure of the Jumper setting on Coordinator. 

I have flashed the ZNP hex image that is available in Z-stack folder onto the CC2530 using SmartRF Flash programmer and flashing is always successful. So I assume CC2530 work fine. 

Can you please suggest me where I have got the problem? Any help or suggestions are appreciated. 

Thank you. 

Best,

Vidya.