Hi, I see in CC Debugger user's manual that duplicate it is possible.
Is it legal and free to duplicate CC Debugger ?
Thank you !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I see in CC Debugger user's manual that duplicate it is possible.
Is it legal and free to duplicate CC Debugger ?
Thank you !
I can answer that one. Anyone that has had to rely on an external programmer probably has a few fried ones laying around!
The first thing I did when I got my CC Debugger was flash a CC chip with the source code and made myself a spare CC Debugger.
Why wouldn't you should have been your question.
Hi.
I want to make my own tool because PCB prototyping in my country is pretty cheap.
All I want to ask for legality.
Thank.
On a general basis, please refer to the Terms of Use on the TI web (http://www.ti.com/footer_terms) and the Software License Agreement you agreed to when downloading the source material.
For the debugger, we do not contractually prohibit reusing or even duplicating the hardware design, but note that once you combine the design with the TI-owned debugger firmware, for which no redistribution rights are granted, the combination can only be used for personal or non-commercial purposes.
Br,
ABO