Other Parts Discussed in Thread: CC2530
Hi,everyone
Can I use the cc2530 timer 4 in this way?Below is my code.I want to use timer 4.For example , i want to delay 13us , but watching the pulse in the oscilloscope,
while(1){
P0_6 ^=1;
Time4_wait(13);
}
the time is not right .The actual time is about 22us.
void Time4_wait(uint16 t)
{
static uint16 m,n,i;
n = t%255;
if(t >= 255){
m = t/255;
for(i=0;i<m;i++){
T4CTL |= (1<<2); //add by stones
T4CC0 = 255;
T4CTL |= 0x10;
while((TIMIF & (1 << 3)) == 0)
{}
T4CTL &= ~0x10;
T4CTL |= (1<<2); //counter clr
TIMIF &= ~(1 << 3);
}
}
if(0!=n){
T4CC0 = n;
T4CTL |= (1<<2); //counter clr
TIMIF &= ~(1 << 3); //flag clr
T4CTL |= 0x10;
while((TIMIF & (1 << 3)) == 0)
{}
T4CTL &= ~0x10; //suspend
T4CTL |= (1<<2); //counter clr
TIMIF &= ~(1 << 3); //flag clr
}
}