This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530 WDT interval question

Other Parts Discussed in Thread: CC2530, Z-STACK

Has CC2530 support more than 1 sec WDT interval, i had study the WDCTL (0xC9) – Watchdog Timer Control, the max Timer interval only support 1 sec,

i has use the WatchDogEnable( 0x00 );  // 00: Clock period × 32,768 (~1 s) when running the 32-kHz XOS

then set the WDCTL.CLR to clear the timer,

WD_KICK()         st( WDCTL = (0xA0 | WDCTL & 0x0F); WDCTL = (0x50 | WDCTL & 0x0F); )

but the one second WDT interval is too short, 

if i want to rebot after 10 secs, how can i to set up the register?

Thanks