Other Parts Discussed in Thread: CC2520, MSP430F2619, MSP430F2618
hi all
i m trying to run zstack on msp430f2619+cc2520 custom board
i used msp430f2619.xcl form iar ide folders as a linker file. instead of default msp430f2618.xcl
when i try to compile i m getting the below error
Building configuration: GenericApp - EndDevice
Updating build tree...
Linking
Error[e16]: Segment DATA16_N (size: 0x802 align: 0x1) is too long for segment definition. At least 0xbe more bytes needed. The problem occurred while processing the
segment placement command "-Z(DATA)DATA16_I,DATA16_Z,DATA16_N,DATA16_HEAP+_DATA16_HEAP_SIZE=1100-20ff", where at the moment of placement the
available memory ranges were "CODE:19bc-20ff"
Reserved ranges relevant to this placement:
1100-1189 DATA16_I
118a-20ff DATA16_Z
Error while running Linker
Total number of errors: 1
Total number of warnings: 0
what i need to do... kindly. help...
if anybody have proper xcl file kindly provide..
thank u