Other Parts Discussed in Thread: CC2530, CC2540
Hi,
I have tried to set the timer 3, and I don't know what i am missing. I need to do an interrupt every 5 ms. If anyone can help me would appreciate it. My code is the following:
PERCFG = 0xC0;
P2SEL |= 0x20;
P1SEL = 0x18;
P1DIR |= 0x18;
T3CTL = 0x1A;
T3CCTLO = 0x64;
T3CC0 = 0x0A;
I focused first on the configuration of timer 3 is something that so far I have not set. Thanks for your help.