Other Parts Discussed in Thread: CC2530
dear all
I have some CC2530 boards,when i use one of the boards works as coordinator,and the other work as end devices,the end device can start smoothly success.But,when i use anther boards work as coordinator,i discovery end device can't join the network,the device state is DEV_NWK_DISC.
I try to use an external power supply to the board, and the phenomenon is as the same as using the CCdebugger to supply the power to the board.
This circuit boards are the same,and the chips are cc2530,and they are all the same batch.
I am very much looking forward to your help;
regards!