This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem when reestablishing lost links

Other Parts Discussed in Thread: CC2530

I am working with cc2530 with zstack.
I have two bound devices. When distance between devices is small each device can send message to another device.
When distance between devices becomes bigger than 10m, the connection between the devises disappears and devices cannot communicate.
When I put devices again togeter they DO NOT reconnect automatically.

I need to make it so, that when moving devises together the lost connection should be reestablished.

Please andise me, how can I do so.

Thanks.

P.S.   The problem of reestablishing broken connections still persist.

If this feature is not available, and existing frameworks do not help solving this problem,

then what reason to use this protocol?

Please advice.

Thanks.