This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530ZNP. Unknown Status byte value in AF_DATA_CONFIRM command

I´m using ZNP (ZStack version 2.5.0). I have tried to send some  AF_DATA_REQUESTs to and end device mostly without problems, but sometimes I have received a AF_DATA_CONFIRM command with Stauts = 0xF0. I can´t find this value at ZigBee PRO Networ Processor datasheet about.

What's the meaning of the 0xF0 Status?

  • Sounds like these data requests are to a sleeping end device that does not wake up often enough?

    #define MAC_TRANSACTION_EXPIRED     0xF0  /* The associate response, disassociate request, or indirect
                                                 data transmission failed because the peer device did not respond
                                                 before the transaction expired or was purged */