Other Parts Discussed in Thread: Z-STACK, CC2530EM, CC2590, CC2530-CC2591EM-RD, CC2530
Hello,
I have been struggling with this for a few days, and went through all posts in the forum, but could not resolve my issue:
I am having problem with the sampleapp in ZStack-CC2530-2.5.1a
I followed the instructions in Z-Stack User's Guide - CC2530DB.pdf
-I can build and compile the project in IAR
-I can program the boards (I have two boards), I use a jumper for coordinator at pins 9-11
-When I turn the coordinator on, first LED1 (green) flashes and LED3 (yellow) stays on, then LED1 turns off, and LED3 is still on, and I can see "ZigBee Coord Network ID: XXXX" on the LCD, but then after a few seconds, LED3 turns off (unlike what the document says) but the LCD still shows the "ZigBee Coord..." Message.
-I turn the router on, first LED1 with flash and LED3 stays on, then LED3 turns off and LED1 keeps flashing. On the LCD, I can see the MAC address of the boards "IEEE: XXXXXXXXXXXXXXXXXX", but LED1 never stops flashing, and Coordinator does not react and all LEDs are off on Coordinator. The boards are on the same desk right beside each other.
-I have also attached packet sniffer's output, which shows some packets but the node never join the network.
I appreciate any help
Sina