Other Parts Discussed in Thread: CC2530
I'm running ZStack 2.5.0 on a CC2530 platform. I have a server (PC), coordinator/gateway and 65+ routers. In my application, the routers do not communicate with one another, except during OAD. I was looking at adding Many-To-One in the ZStack Developers Guide and was wondering if this feature would affect OAD, since I have parents (and uncles per se) upgrading children.
I would guess that as long as a node was a neighbor to the child, OAD would work fine. Is this correct?
From ZStack Developers Guide:
Many-to-one routing is a special routing scheme that handles the scenario where centralized traffic is involved. It is part of the ZigBee PRO feature set to help minimize traffic particularly when all the devices in the network are sending packets to a gateway or data concentrator. Many-to-one route discovery is described in details in Section 5.4.