Hi All,
I am using cc2530ZNP mini kit.
I have coordinator and 2 end-devices. When all end-devices are located not far from coordinator everything works OK. However when I bring one of my end-devices rather far from coordinator (about 12-15 meters), it cannot communicate with coordinator.
I would like to increase the communication distance between end-device and coordinator.
How can i do that?
It is possible to change the TX POWER using AF ZDO api? How can I do that?
I am using the simple application cordinator af zdo/ end devices from TI. There is any command to change the TX power in order to increase the distance?
Regards
Ramiro