I am using a ProFLEX module (CC2520-CC2591). I would like to implement a CCA mode which complies with 802.15.4 CCA Mode 2 (Carrier Sense only). Looking at the CC2520 Datasheet (cc2520.pdf), I am not sure how I can achieve that.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC2520
I posted this in Low Power RF Hardware & Tools Forum but maybe this is the right forum.
Let me elaborate a bit.
CC2520 offers 4 CCA modes by setting CCACTRL1 bit 4:3 to the following:
00 : CCA always set to ‘1’
01 : CCA = ‘1’ when RSSI < CCA_THR-CCA_HYST, CCA = ‘0’ when RSSI >= CCA_THR
10 : CCA = ‘1’ when not receiving a frame, else CCA = ‘0’
11 : CCA = ‘1’ when RSSI < CCA_THR-CCA_HYSTand not receiving a frame, CCA=0 when RSSI >= CCA_THR or receiving a frame
Compared to 802.15.4 CCA modes:
CCA Mode 1: Energy above threshold. CCA shall report a busy medium upon detecting any energy above the ED threshold.
CCA Mode 2: Carrier sense only. CCA shall report a busy medium only upon the detection of a DSSS signal. This signal may be above or below the ED threshold.
CCA Mode 3: Carrier sense with energy above threshold. CCA shall report a busy medium upon the detection of a DSSS signal with energy above the ED threshold.
It seems to be CC2520 does not offer an option to use Carrier sense for CCA?
Or I see, sorry for my misunderstanding, I don't quite understanding your claim"CC2520 does not offer an option to use Carrier sense for CCA", CCA modes are provided, why it dose not offer CCA?
in your case, CC2520 CCACTRL1 bit 4:3 [01] = CCA mode 1 in 802.15.4, CC2520 CCACTRL1 bit 4:3[10] = CCA mode 2 in 802.15.4, CC2520 CCACTRL1 bit 4:3 [11] = CCA mode 3 in 802.15.4
Rui