Other Parts Discussed in Thread: CC2591, CC2530
hi all,
in my system, i use CC2530+CC2591, and i have use the following code to change the TXPOWER,the code is as follows:
// Initialize the MAC
ZMacInit();
uint8 value = 0xE5;
MAC_MlmeSetReq(MAC_PHY_TRANSMIT_POWER, &value);
however,when i test the current consumption,it only 101~108 mA, but from the materials , i found it should about 166mA.
how can i do to change the tx power, could you give me help?
thanks