Other Parts Discussed in Thread: CC2530
What is file C:\Texas Instruments\CC2530ZNP Mini Kit\Bin\ Simple Application - Coordinator Text Document 15 KB
How can i use it? Is it the file which should be flashed into device marked as "Coordinator". If so, why it is not HEX file as i supposed should be.
The same related to "Router" and "End Device".
First three line of "coordinator" opened with WordPad are as follows
@8000
23 25 30 32 75 3A 20 47 72 70 25 30 34 78 20 43
6C 75 73 25 30 34 78 2C 20 53 72 63 41 64 25 30
which is definitely not Intel HEX file..
Thanks
Edward