Other Parts Discussed in Thread: CC2530, Z-STACK, CC2430
Hi all,
I would need to get an old version of the Z-Stack software for the CC2530 platform; the version is 2.4.0, where could I get it?
Thanks in advance,
Antonio
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a reason for you being interested in an older Z-Stack version?
Are planning to port to 2.5.1a?
LPRF Rocks the World
HI,
well I'm working on an old project based on the 2.4.0 version. I would have the original source unmodified as reference, so i could migrate to the 2.5.1 version then.
Thanks
Hi,
We're facing the same problem. We have a legacy project based on ZStack 2.4.0 and we need to isolate code in order to perform a cleaner migration. Is it possible to download the 2.4.0 to have as reference?
Thanks and best regards
It would probably be good for TI to have a link on the site to previous Z-Stack releases, of course with a big warning like "These are old - use them at your own risk - upgrade soon!". I have a client that is using ZB2006 on CC2430 and it would be handy to be able to grab this release, fully knowing that it's obsolete.
--Derek
Hi guys,
I found the old sources here, modifing the zstack 2.5.1 download url.
http://www.ti.com/lit/zip/swrc125d
or
https://www.ti.com/general/docs/mytilit/getmytiliterature.tsp?lang=en&baseLiteratureNumber=swrc125d&fileType=zip
it's unbelievable that TI don't provide any link to it nor support to oure requests.
Hope this was helpful.
Enjoy
Hi guys,
I take these inputs are very valuable feedback; please understand we always suggest our customer to use the latest stack releases because they follow the latest enhancements at profile and stack level therefore we post only the latest one on the web.
I opened up an FTP server where I posted the 2.4.0 on 2530.
Thanks,
TheDarkSide
The files from the dropoff area available for 3 days.
1. Open an ftp session to ftppickup.ti.com.
ftp ftppickup.ti.com
2. Login with the userid 'pickup'.
Name: pickup
3. Enter the password.
Password: piurh!
4. Change directories to the pickup directory.
ftp> cd /pub/share/ligoohe
Note: If you are using a graphical ftp client, you will not
see the hidden pickup directory name ligoohe appear
in the file list. You will need to use a manual
'Change Directory' or 'CD' command to change into the
dropoff directory.
5. Set the file transfer mode to ascii or binary as necessary.
ftp> bin
6. Transfer the file.
ftp> get <file>
7. End the ftp session.
ftp> quit
Hi TheDarkSide and others,
I was wondering if this link could be opened again? I need to get an old version of ZStack for the CC2530, or a version that will work with IAR8051 v8.10.
We also have a legacy project & situation that requires an older version.
Thanks.