This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ZStack SimpleApp Modification

Hello,

I'm trying to utilize the SimpleApp that was packaged with ZStack to collect A/D measurements from sensor nodes and output them to the UART of the coordinator.  If I'm reading the documentation correctly, the SimpleApp is set up to do exactly that.  I have a different board configuration and have modified hal_board_cfg.h to reflect changes such as LEDs etc.  It seems that the coordinator starts up correctly as LED3 blips once then stays on (I only see a beacon request in the Packet sniffer though, followed by the 15second interval message)  

The end device appears to start correctly, however LED3 blips continuously and MY_FIND_COLLECTOR_EVT trips every ~30 secs.  I've attached the packet sniffer log.

Any help would be greatly appreciated.

Thanks,

Tyler

3414.sniff.psd