Hi I'm working on a Zigbee SE product using cc2531DK_Dongle. My question is regarding the certicom certificates. I noticed there is some certificate data pre-loaded, the implicit cert includes a text string "TESTSECA", however when testing with a device loaded with a certicom test certificate the CBKE gets terminated by the trust center after the Ephemeral Data Request.
I reviewed the certificate NV initialization and I see it is read from the same flash lock page that stores the IEEE address. Does this cc2531DK_Dongle come preloaded with a valid test cert from certicom?
What is the recommended method to program the certificate if I wish to switch the device to a certicom test certificate ? Is there an MT procedure for writing the IEEE flash pages?