This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

usblib on cc2538DK

Other Parts Discussed in Thread: CC2538

Hi,

I am building a usb interface for cc2538. Can I use the cc2538dk to test it?

Is there a sample breakout schematic I can use?

Thanks

  • Hi QW,

    from a SW standpoint, have you checked USB examples available at http://www.ti.com/tool/cc2538-sw ?

    These contain usblib:

    usblib: Complete software framework to take full advantage of the USB device controller on the CC2538. The library implements all the standard USB requests and provides hooks to support any USB device class implementation. The library comes with examples for a USB CDC-ACM (serial port) device and a simple HID device.

    Thanks,

    TheDarkSide

  • Hello ,

    I have downloaded the same Software and working with CDC USB Driver. I am not able work with the software.
    As software says that there is a COM Port loopback, but I am not able to work with the Software.

    Do I have to open the COM ( Windows) Terminal to send and receive the data. Please let me know how can I proceed on the same.

    Regards,
    Gaurav Kumar