This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Avoiding time critical operations with NV writes

OSAL API SWRA194 Version 1.11 states:

These are blocking function calls and an operation may take several milliseconds to complete. This is especially true for NV write operations. In addition, interrupts may be disabled for several milliseconds. It is best to execute these functions at times when they do not conflict with other timing-critical operations. For example, a good time to write NV items would be when the receiver is turned off.

What is the best means to determine when the receiver is turned off?  Thanks.