This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSR ProFLEX01-R2 with Z-Stack

Other Parts Discussed in Thread: Z-STACK, CC2591, CC2520, MSP430F5437A

Hi All

We are in the middle of integration of ZigBee Pro with the LSR based on Z-Stack

Recently we have downloaded the Z-Stack code , imported it to be used with LSR ProFLEX01-R2 (which uses MSP430F5437A+CC2520 & CC2591) . 
We are working with IAR-IDE 5.40.
We have performed all the changes according to "ProFLEX01_ZigBee_PortingGuide_and_SampleApp_330-0039-R1.0.pdf". The module receives & transmit few 100`s of cycles and then we are experiencing a RESET.
  • Has anyone experienced such a phenomena?
  • Are there any newer version of Z-Stack that correct this kind of problems?
  • Can you suggest ways of detecting the problem (please be aware that the MAC low level source code is not at our disposal, since it was not included in the Z-Stack downloaded from TI site)?
  • Can you offer a way of bypassing this issue , in order to continue the development tasks and solve this issue later?

Waiting for your replay
Sincerely 

Shai

  • Hi friends, 

    I have ported the MSP430F5438A+CC2520 experimantal board zstack to LSR-ProFLEX01 zigbee module. 

    In experimental code, There are 6 GPIO from cc2520 connected to MSP430. 

    But In LSR-ProFLEX01 zigbee module, only 3 GPIO connected to msp430. 

    What are the changes needed for this? 

    Please guide me to port this.

    Regards, 

    Keerthi G

  • Keerthi,

    I noticed you started a new thread for this question. Kindly request you to not post duplicate queries.

    Thanks,

    Saurabh

  • Hi Mr.Saurabh Narang,

    They have posted a question what i am asking.

    They posted this thread 31-07-2013.

    In case they have solved this issue, it may help for me. 

    If I posted here, they will receive the mail . So that I posted here too. 

    Is there any problem for this? 

    If so, sorry. 

     

    Regards, 

    Keerthi G

  • Hi!

    I am also working with LSR ProFlex01-R2 and I would like download the Z-Stack code to be used with LSR ProFlex01-R2. Where can I download the Z-Stack code? I would also like to know where I can obtain the document "ProFLEX01_ZigBee_PortingGuide_and_SampleApp_330-0039-R1.0.pdf".

    Thank you so much!


    Best regards,

    Paula.

     

  • Hi,

    You can download zstack from here: http://www.ti.com/tool/Z-Stack

    and 

    porting guide from here: http://www.lsr.com/downloads/products/wiki/ProFLEX01%20Porting.txt

    Regards,

    Keerthi G

  • Thank you. I have already downloaded the Z-Stack Energy, but I want to know what code I have to load in the PorFlex01-R2 to be used with the ZigBee standard or if I have to build the code to load in the ProFlex.


    I would also like to know the communication protocol, i.e, the format of the frames to comunicate with modules and the configuration to setup the modules as a coordinator, router or end device.


    Thank you.


    Best regards,


    Paula.