Other Parts Discussed in Thread: CC2531EMK
Hello,
I have one ZNP coordinator and one ZNP router. MAC ACK works but APS ACK fails. In such a simple network (no other devices) why would APS ACK fail but MAC ACK work?
Thanks,
Derek
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC2531EMK
Hello,
I have one ZNP coordinator and one ZNP router. MAC ACK works but APS ACK fails. In such a simple network (no other devices) why would APS ACK fail but MAC ACK work?
Thanks,
Derek
Do you use AF_ACK_REQUEST option when you call AF_DataRequest?
Do you also check the return value of AF_DataRequest? Check if the return value is ZSuccess first.
HI Dereck,
can you please also check or attach the sniffer log?
I would like to see if APS ack mode was requested OTA.
Thanks,
TheDarkSide
Hello,
I finally figured it out. There was a mismatch in the security settings between the two devices. One device had security = 0, the other security = 1. That allowed one way communications but not bidirectional communications. It also explained why MAC ACKs would work but APS ACKs failed. I bought a CC2531EMK for the client and once they ran the packet sniffer and sent it to them we saw the problem.
Thanks for your help!
--Derek