hi everybody, I'm trying to work example: ZigBee Lighting Gateway SW. I flash my cc2531 whit SampleGateway-USB-SBL.bin and run in ubuntu 12.04 server and client examples, the client is listDevsCmdLine but i cant conect any zlight devices on my Zigbee network.
i try whit:
- Press the S1 button on the CC2531EMK dongle, the RED LED will flash for 60s during which time devices can associate the the network.
- Follow the device specific instructions for other ZigBee devices to make them join the ZigBee network.
- For Zlights you need to:
- Hold the button for 3s to reset it to factory new and wait for 5s until the LED's blink (this step can be skipped if the ZLight is already factory new).
- Hold the button for more than 10s to make it join a network
in my ubuntu server program example i see this:
in the client:
IP addresses for 127.0.0.1:
IPv4: 127.0.0.1
Trying to connect...
Connected.
in the server:
Message from Socket Sever
zllMain: waiting for poll()
thanks